Requires Option SNC
This topic describes how to make cable connections between Leader and Follower(s) in a multi-instrument setup using the Basic Sync cabling method.
Rear Panel Cabling
For multi-instrument systems with greater than two instruments:
The order of entries added for Followers in the software GUI must match the cabling order in which you have connected the Followers.
Connect the 10 MHz REF OUT connector of the Leader to the 10 MHz REF IN connector of Follower <1> using a clock cable.
Connect the 2.4 GHz OUT connector of the Leader to the 2.4 GHz IN connector of Follower <1> using a clock cable.
If there are more than one Follower in the setup:
Connect the SYNC DN connector of the leader to the SYNC UP connector of Follower <1> using a KDMI cable (a u-HDMI cable with non-standard pin assignments).
If there are more than one Follower in the setup, connect the SYNC DN on Follower <1> to SYNC UP on Follower <2>.
Repeat step 5 so that all remaining Followers in the setup are connected to their next Follower in the setup.